AKD Capture Engine Configuration
The AKD capture engine provides a broad range of capabilities for configuration of the capture events.
- It is capable of configuring preconditions to allow the application programmer to specify sequential events or conditions that must be met before the capture event can be triggered.
- The capture Engine in the AKD is configured with SDO #0x3460 (subindexes 1 to 10).
- The AKD supports two capture engines (0 and 1); the application programmer must configure the desired engine.
Sub Index Zero pulse (zero signal) of a hardware pin such as digital input or feedback pin. # |
Function |
---|---|
1 |
Trigger for capture engine 0. |
2 |
Trigger for capture engine 1. |
3 |
Mode for capture engine 0. |
4 |
Mode for capture engine 1. |
5 |
Capture Event for capture engine 0. |
6 |
Capture Event for capture engine 1. |
7 |
Precondition edge for capture engine 0. |
8 |
Precondition edge for capture engine 1. |
9 |
Preselect for capture engine 0. |
10 |
Preselect for capture engine 1. |
AKD Configuration Parameters
These are the configuration parameters for the ADK capture engines.
For more details, see either CAP0.PRESELECT or CAP1.PRESELECT.